Periodicity

The period of execution of a pipe is the time spent between two successive computations of set values for the same pipe. The period of execution of a pipe is specified by the PERIOD parameter of the input Pipe Block.

Set the Period of Execution

Figure 4-48: Set the Period of Execution

All the pipe values are computed independently of events and sequences execution.